paramax reducer

Robust & Durable Large Industrial Gearboxes

paramax.png

PARAMAX®

  • Up to 5,230 HP (3,900 kW) 
  • 58mm to 360mm (Hollow & Solid) 
  • Up to 4.9m Ib•in (552,000 N•m) 
  • Up to 500:1 Standard
Hansen Multistage

Hansen P4 Multistage - Horizontal

  • Up to 14,080 HP (10,500 kW)
  • 3.15in to 15.75in (Solid Shaft)
  • Up to 9.7m Ib•in (1.1m N•m)
  • Up to 630:1 (and custom ratios)

Hansen P4 Multistage - Vertical

  • Up to 14,080 HP (10,500 kW)
  • 3.15in to 15.75in (Solid Shaft)
  • Up to 9.7m Ib•in (1.1m N•m)
  • Up to 630:1 (and custom ratios)

Hansen P4 UniMiner

  • Up to 2330 HP (1738 kW)
  • Up to 889,000 Ib•in (100,445 N•m)
  • 8:1 to 71:1

Robust Gearbox Solutions for your Industrial Operations

Sumitomo's Large Industrial Gearboxes feature easily accessorized and customizable standard line of speed reducers for your demanding heavy-industrial applications.

Powered by a robust, proven design, our gearboxes and reducers are rugged, flexible, and economical to operate. We have a wide range of options available to find the perfect fit for your operations.  We have the perfect solutions for your most demanding applications. The Hansen vertical gearbox offers the best features required for heavy-duty and long-running applications.

  • Proven Reliability: With over 80 years of experience, Sumitomo Drive Technologies has a longstanding reputation for providing world-class gearmotors, gearboxes, and speed reducers.
  • Durability: Rugged housing and state-of-the-art technology provide remarkable power and withstand the harshest environments.
  • Wide Size Range: We offer the widest range of large industrial gearboxes on the market. 

Choosing the right large industrial gearbox for your application starts with asking the right questions. Our customers are our top priority, and we strive to meet their needs by offering modifications or custom options.

Find Your Perfect Gearbox Solution Today

Get Your Large Gearbox Quote Now

Fill out the form or call us at 1.888.635.6830 to get your personalized gearbox quote and take the first step toward optimizing your operations for success.


Why Industrial Companies Choose Us

With over 130 years of engineering expertise, Sumitomo Drive Technologies is a trusted global leader in power transmission solutions.

Custom Fit Solutions

Sumitomo Gearboxes can be tailored to meet specific operational needs with custom options from mounting options, to motors and more.

Rugged Durability

Built to withstand the toughest conditions, our gearboxes feature rugged designs that deliver reliable performance in even the harshest environments.

us-based engineering support

Trust our US-based engineering team and support staff for superior service, faster response times, and solutions tailored to your needs.

Parallel Shaft Gearboxes
Hansen P4s
uniminer
uniminer
Parallel Shaft Gearboxes
Hansen P4s
uniminer
uniminer

Enhance Your Operations with Reliable Large Gearboxes

Sumitomo's Large Industrial Gearboxes feature an easily accessorized and customizable standard line of catalogued speed reducers for your demanding heavy-industrial applications. We're the gearbox manufacturer to help optimize your operations. 

Whether you need the strength and flexibilty of our Paramax® 9000 with its wide range of options, or the rugged and heavy-duty of Hansen gearboxes for long running applications, we have the perfect solution that fits your needs.

Our industrial gearboxes are built to deliver dependable performance, improve efficiency, and reduce downtime—helping you keep operations running smoothly.

Success Story | Sumitomo Paramax Drives for Wilpinjong Coal Mine

Industry: Mining

Sumitomo Drive Technologies, Australia, recently supplied complete drive packages to be installed at the Wilpinjong Coal Mine Site located Northeast of Mudgee in NSW. The team responsible for both the design and installation of infrastructure is made up of a joint venture between Theiss and Sedgeman. Sumitomo Drive Technologies delivered eight complete drive packages ranging in size from 45kW to 280kW for use on the conveyor systems.

All drive packages were assembled on specially designed base plates, and are complete with motors, fluid couplings or grid type couplings on the reducer inputs, shrink disc rigid couplings on the outputs and all guards. After workshop assembly all were laser aligned and subjected to a no-load test run using Sumitomo Drive Technologies' purpose-built test rig before final inspection and delivery to the site. Sumitomo Drive Technologies' Managing Director, Steve Wightman said, "We are delighted to be awarded the supply contract for this Greenfield Mine Site project. This is the first time we have worked with Thiess Sedgeman and look forward to a long association with both companies." He added, “We believe our success in this instance is due to our promotion of quality power transmission products and ability to customize those products to our clients' needs.”

The Paramax range is one of the most comprehensive available on today's market, comprising 26 standard frame sizes, all available in a number of configurations as well as a specially designed cooling tower fan drive. Parallel offset or right-angle types with solid or hollow output shafts are available. Additions such as Labyrinth or taconite sealing, backstop options and if noise emission is a problem, the option of precision ground bevel sets on the high-speed reducer inputs will drastically reduce the noise levels.

Sumitomo Drive Technologies is one of the world's largest gear manufacturers. It offers a range of reducers and gear motors for all applications, and its `Seisa Gear division' has the ability to engineer special design gear reducers or speed increasers up to 10,000 kW.

Success Story | Coal Handling Conveyors for the Mining Industry

Challenge

Responsible for purchasing and organizing supplies for this coal mine, the maintenance planner found that it was becoming increasingly more difficult to find and gather parts to fulfill internal orders. To overcome this challenge, the mine decided to create a program to simplify the ordering of spare parts and spare kits.

The facility wanted to partner with a manufacturer who could provide engineering, customer service and maintenance expertise to support the current program. Sumitomo Machinery Corporation of America (SMA) began creating a plan to meet and exceed the customer's expectations.

Solution

Multiple members of the Sumitomo team worked hard to accomplish the end user's goals. Sumitomo implemented a Paramax binder project for the account, featuring an organized configurator price quote with a competitive multiplier for distribution. Sumitomo strengthened the personal relationship with machinery lubrication, long-term prep, and hands-on local support. 


Results

To solidify the partnership with the end user, SMA's team members were invited to participate in a spring seminar between the coal mine and power generating company.

The efforts that SMA made over the two-year span with the customer produced about $1.3M in purchases. Moving forward, the customer is expected to continue to purchase Paramax spares and replacement units from SMA considering that Sumitomo Machinery Corporation of America was able to deliver the ideal solutions to meet the needs of the end user.

"A long term prep procedures guide and program will help us ensure our recently purchased Paramax units are correctly stored and maintained."-The Customer, Marissa, IL

Success Story | Sumitomo-Hansen's P4 UniMiner is a Good Fit with West River Conveyors

West River Conveyors & Machinery Company (www.WestRiverConveyor) is a leader in custom-built, custom-designed belt drives for coal and potash applications and is one of Sumitomo-Hansen’s largest P4 UniMiner drive consumer. 

Sumitomo-Hansen’s P4 UniMiner drives are used on many of West River's belt drives based on the flexibility and high customer satisfaction of the products.  Customers find benefit in the universal and flippable mounting features of the P4 UniMiner, eliminating the need to buy reducers specifically oriented for each installation.  This is a great advantage to users wanting to purchase spares for future changeouts where one reducer covers all orientations. 

“The design layouts and features of the UniMiner Drive work well with our application”, states Jerry Roulett, President of West River.  “The selection of sizes and offerings available per HP and RPM for the Hansen P4 UniMiner Drives  fit the needs of West River’s applications perfectly.  “We have had great customer acceptance with the P4 UniMiner. Customers who have installed our drives in their operations will speak highly about the quality of the reducers.  We’ve been using Hansen UniMiners on our belt drives for over a decade now.”


West River’s Purchasing agents especially like the working relationship they have with Sumitomo-Hansen.

“Sumitomo-Hansen’s ability to service West River is exceptional.  Our Sales Manager makes regular visits to our shop and is excellent to work with.  The factory works directly with our Purchasing Manager to meet our deadlines even when the deadlines seem very tight. Most of all, the quality products produced by Sumitomo-Hansen coupled with excellent customer service make it easier for us to continue to use Sumitomo-Hansen products on our belt drives.” - Tina Clevinger, Purchasing

Sumitomo-Hansen strives to meet the unique requirements for bulk material handling and mining applications in order to position our customers as industry leaders.

aftermarket_why_choose_collage

Ready to Keep Your Operations Running Strong?

Ready to take your operations to the next level with dependable, high-performance gearmotors? Whether you need a standard solution or a custom-fit design, Sumitomo Drive Technologies has you covered.